Keep your Crew Warm: Cold-Weather Essentials To Maintain Productivity
The cold weather is coming. As winter approaches, keeping your crew warm is absolutely essential. When it comes to cold, we tend to think of the challenges of outdoor work environments. But cold temperatures also affect indoor settings like warehouses, corporate offices, and industrial facilities. Ensuring your team is properly equipped for the winter months is key to maintaining high morale and efficiency, no matter where they’re working. Let’s explore the best ways to protect your crew from the cold and create a work environment that promotes comfort and safety.
Why Cold Protection Is Important
There’s a strong connection between temperature and productivity. Studies have shown that for every degree below 50°F, worker productivity falls by 1%. This means that a crew working in 40° temperatures are operating at 90% efficiency. Cold environments can slow down operations and cause fatigue and discomfort, negatively affecting overall morale.
Beyond productivity, the risk of cold stress is a real concern. The Occupational Safety and Health Administration (OSHA) recommends employers protect workers from cold stress, which can lead to conditions like hypothermia, frostbite, and immersion. It is not just low temperatures that present health risks. Wind, rain, and damp conditions can amplify the risks. Pre-existing health conditions and poor physical conditioning also heighten a person’s vulnerability to cold stress. Keeping your eye out for early signs of cold-related illnesses like hypothermia, frostbite, and immersion can go a long way in protecting your people. To learn more about recognizing and preventing cold stress, check out this article on cold stress from Global Industrial’s Knowledge Center.
There are two primary strategies for keeping your team warm and productive: providing proper winter work gear and ensuring the work environment is adequately heated. Here’s what you need to know.
Dressing for Success in Winter Work Gear
Wearing the right cold-weather gear is the first step in ensuring workers remain safe and comfortable. Let’s break down the essential winter work gear for your crew:
Cold-Weather Gear
Moisture-Wicking Clothing (Base Layers)
The innermost layer of clothing should wick moisture away from the skin to keep workers dry. Damp skin cools much faster, increasing the risk of cold stress.
Insulated Coveralls and Bibs
Insulated coveralls or bibs provide full-body coverage and are designed for maximum warmth. They’re perfect for workers exposed to outdoor environments for extended periods, ensuring that no gaps in clothing let in cold air. For workers in hazardous environments, flame-resistant coveralls offer both protection from fire and insulation from the cold.
Wind and Rain Resistant Jackets
Layering is key. A wind and rain resistant jacket is the outermost layer that protects workers from harsh winter conditions. These jackets are designed to repel moisture and block wind, preventing exposure to the elements while keeping the inner layers dry and warm.
Insulated Vests
Wearing an insulated vest over base layers provides warmth without restricting movement, making them ideal for workers who need mobility while keeping their core warm.
Hats and Face Masks
Since a large portion of body heat is lost through the head, insulated hats are essential for maintaining warmth. Face masks or balaclavas can protect the nose, cheeks, and mouth from frostbite in extremely cold conditions.
Gloves and Insulated Boots
Cold-resistant gloves are a must for keeping hands warm and functional in freezing temperatures. Insulated boots provide much-needed warmth for the feet, especially for workers standing in wet, cold conditions for long periods.
Hand & Toe Warmers
Ideal for supplemental warmth of your extremities in cold working environments, hand and toe warmers are typically designed for single-use applications, so they can be disposed of after your day of work.
Specialty Winter Work Gear
Certain jobs require specialized winter gear. For example, workers operating near traffic or heavy equipment may need high-visibility cold-weather gear, while those in environments with sparks or open flames should wear flame-resistant coveralls. These garments not only keep workers warm but also provide essential protection from specific hazards. Explore more cold-weather gear options in the cold weather protection section of Global Industrial’s website.
Heaters: Warming the Workspace
While the right gear helps workers withstand cold temperatures, heating the workspace itself is just as important for comfort and productivity. Depending on your work environment, different heating solutions may be required. Global Industrial offers a wide variety of industrial heaters to meet the needs of various settings.
There are three basic types of heaters:
- Radiant Heaters: These heaters warm objects and people directly rather than heating the surrounding air, making them highly effective in open or outdoor areas.
- Convection Heaters: Ideal for indoor use, convection heaters warm the air and circulate it throughout the space.
- Forced Air Heaters: These powerful heaters blow warm air to quickly raise the temperature in large areas like warehouses or outdoor worksites.
Let’s take a deeper dive into the specific types of heaters that may work for you:
Portable Electric Heaters
For smaller indoor areas like offices, workshops, or break rooms, portable electric heaters are an excellent option. These heaters are easy to move, allowing you to bring warmth where it’s needed most. They are perfect for temporary or supplemental heating in spaces where centralized heating isn’t practical. Depending on your needs, there are a variety of options: portable and space heaters. These smaller heating solutions provide quick, localized heat and are a cost-effective solution for maintaining a comfortable temperature.
Larger facilities such as warehouses, manufacturing plants, or garages require more powerful solutions. Industrial heaters—which include unit heaters, process heaters, and forced-air heaters—are built to warm large areas efficiently. These heaters provide consistent heat across wide spaces and are designed to withstand heavy-duty use.
Gas and Oil Heaters
For outdoor job sites or larger spaces without access to electricity, gas and oil heaters are an effective solution. Portable gas heaters and infrared space heaters are commonly used on construction sites or in loading areas to provide immediate, direct warmth. For indoor sites, unit heaters and vent free room heaters are a good option. And don’t forget about the power and reliability of a furnace.
Steam and Hydronic Heaters
In industrial facilities with access to steam or water systems, steam and hydronic heaters provide steady, energy-efficient warmth. These heaters are often used in large indoor spaces where consistent heating is required. There are several types to consider: a simple steam and water unit, a hydronic or wall hydronic unit, or baseboard heater - all great, efficient options.
Specialty Heaters
For your unique needs, you may need a specialty heater. Perhaps you need a wall unit or a fire stove heater for that classic cozy feel. Waste oil heaters are eco-friendly units that recycle used oil to generate heat, making them a sustainable option for businesses that produce waste oil. For outdoor break areas or hospitality environments, patio heaters and fire pits create warm, inviting spaces where workers can relax between shifts.
Keeping your crew warm and productive during the winter months requires a combination of proper winter work gear and reliable heating solutions. From gear to heaters, it’s crucial to provide the right tools to combat cold temperatures. A warm workforce is a safer, happier, and more efficient workforce. For more information on cold weather protection, visit Global Industrial.com.
The information contained in this article is for informational, educational, and promotional purposes only and is based on information available as of the initial date of publication. It is the reader’s responsibility to ensure compliance with all applicable laws, rules, codes and regulations. If there is any question or doubt in regard to any element contained in this article, please consult a licensed professional. Under no circumstances will Global Industrial® be liable for any loss or damage caused by your reliance on this article.